Add an HMI Device
To control an application,
It can also be embedded into targeted Controllers.
- The KAS-IDE is automatically linked to the KVB HMI development software, and the Modbus addresses are automatically set.
When running the KAS Simulator, an internal HMI editor is also available to debug the application.